Skip to main content
Associate III
March 27, 2024
Solved

blocking vs nonblocking RFAL apis

  • March 27, 2024
  • 1 reply
  • 843 views

Hi, 

I am trying to understand the difference between blocking/non-blocking rfal apis.

 

 

ReturnCode rfalNfcvPollerReadMultipleBlocks( uint8_t flags, const uint8_t* uid, uint8_t firstBlockNum, uint8_t numOfBlocks, uint8_t* rxBuf, uint16_t rxBufLen, uint16_t *rcvLen );

 

 

It seems to me that the above api is a blocking one. How can I achieve the same functionality in a non-blocking way ? 

The reason I am asking this is because it seems that this api is taking too much time to execute (Without the time required to perform I2C read). Is my understanding correct on the RFAL library sequence for the above api ?

  1. RFAL library request ST25R3916 for the requested amount of data.
  2. RFAL waits in a busy wait loop until interrupt pin changes
  3. Once the interrupt pin changes, RFAL library performs read from ST25R3916.

I am concerned about step 2 as it is a busy wait loop and other threads seem to be starving. 

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi

rfalNfcvPollerReadMultipleBlocks is a blocking API. The duration of this call depends on the number of blocks requested. 

You can try to use rfalNfcvPollerReadMultipleBlocks with a smaller number of requested blocks or use a loop of rfalNfcvPollerReadSingleBlocks to avoid a too long blocking time.

Or you can format the rfalNfcvPollerReadMultipleBlocks request and send it through non blocking rfalStartTransceive  / rfalGetTransceiveStatus.

Rgds

BT

1 reply

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
March 29, 2024

Hi

rfalNfcvPollerReadMultipleBlocks is a blocking API. The duration of this call depends on the number of blocks requested. 

You can try to use rfalNfcvPollerReadMultipleBlocks with a smaller number of requested blocks or use a loop of rfalNfcvPollerReadSingleBlocks to avoid a too long blocking time.

Or you can format the rfalNfcvPollerReadMultipleBlocks request and send it through non blocking rfalStartTransceive  / rfalGetTransceiveStatus.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.