Skip to main content
Stinde
Associate II
March 12, 2021
Solved

Capacitive wake-up

  • March 12, 2021
  • 2 replies
  • 990 views

Is it possible to use ST25R3916 capacitive wake-up outdoors? The reading area can be wet, frozen or snow covered.

This topic has been closed for replies.
Best answer by Travis Palmer

Hello Stinde,

When the reader is mounted outdoor using a propper housing there should be no problem for that.

For both, capacitive and inductive wake-up apply the same rule:

If the environment changes ( = temperature, metal in close proximity, moisture (mainly influencing capacitive wake-up),..) then the reader will wake-up.

You can then either use automatic averaging which helps filtering those effects or just re-arm the wake-up if no tag has been found.

br Travis

2 replies

Travis Palmer
Travis PalmerBest answer
ST Employee
March 12, 2021

Hello Stinde,

When the reader is mounted outdoor using a propper housing there should be no problem for that.

For both, capacitive and inductive wake-up apply the same rule:

If the environment changes ( = temperature, metal in close proximity, moisture (mainly influencing capacitive wake-up),..) then the reader will wake-up.

You can then either use automatic averaging which helps filtering those effects or just re-arm the wake-up if no tag has been found.

br Travis

Stinde
StindeAuthor
Associate II
March 13, 2021

Hi Travis,

I was thinking since capacitive wake-up is sensing water in human hand. If there is a layer of water between the sensor and hand, can the capacitive sensor really detect the hand behind the water layer. I know the averaging can help in slowly changing environment, but is the water layer close to sensor plates acting as a short circuit for electric field?

Best Regards,

Stinde