Skip to main content
PGao.1
Visitor II
April 16, 2021
Solved

Card emulation mode for CR95HF

  • April 16, 2021
  • 3 replies
  • 1017 views

I have the X-Nucleo-NFC30A1 with the Cr95HF chip.I used the X-Cube-NFC3 v2.1.0.I have changed the platfrom.h file and I am able to read UUID, but I need the device to be in card emulation mode if i set RFAL_FEATURE_LISTEN_MODE to true

I am getting a linker error:

In file rfal_rfst25r95.c

undefined reference to `st25r95Listen'

undefined reference to `st25r95RearmListen'

undefined reference to `st25r95SetACFilter'

undefined reference to `st25r95SPIGetLmState'

And it seems that this functions are not implemented!

Is there any working example, or documentation to implement card emulation?

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    see https://community.st.com/s/question/0D53W00000arwFy/st25r95-card-emulation for similar request.  I will provide the code to you in private.

    Thanks

    Rgds

    BT

    3 replies

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    April 19, 2021

    Hi,

    see https://community.st.com/s/question/0D53W00000arwFy/st25r95-card-emulation for similar request.  I will provide the code to you in private.

    Thanks

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Lluat.1
    Visitor II
    December 20, 2021

    I also met the same problem, could you also send me the card emulation mode St25r95 demo, this is my email A15211163466@gmail.com ,thank you !thank you !

    STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SPIGetLmState (referred from st25r95_com_spi.o).

    STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95Listen (referred from rfal_rfst25r95.o).

    STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95PollField (referred from rfal_rfst25r95.o).

    STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95RearmListen (referred from rfal_rfst25r95.o).

    STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SPIGetLmState (referred from rfal_rfst25r95.o).

    STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SPISetACState (referred from rfal_rfst25r95.o).

    STM32F401RE_NUCLEO_PollingTagDetect\Exe\Project.axf: Error: L6218E: Undefined symbol st25r95SetACFilter (referred from rfal_rfst25r95.o).

    Brian TIDAL
    Technical Moderator
    December 20, 2021

    Hi,

    I've provided the code to you in a private message.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.