Skip to main content
门旭.1
Associate
June 18, 2021
Solved

CMD_FAILED exception about st25Android SDK: readMailboxMessage()

  • June 18, 2021
  • 2 replies
  • 1144 views

I can use st25DVTag.writeMailboxMessage(bytes) to write the Mailbox,I can also use st25DVTag.readMailboxMessageLength() to get the length of message(it returns 1),but when I try to read the Mailbox message,it throw a com.st.st25sdk.STException: Error CMD_FAILED.

st25DVTag.readMailboxMessage(0, 0) or st25DVTag.readMailboxMessage(0, 1), both of them can occur exception.How can I read the MailboxMessage?

0693W00000BbLqaQAF.png

    This topic has been closed for replies.
    Best answer by Olivier L

    Hi,

    After writting some data in the mailbox, you should wait that the MCU writes an answer. Here, I think that you tries to read the Mailbox before that the recipient gets the time to answer. I can see that the read message length is null.

    After writing the message please use hasHostPutMsg() to monitor if the MCU has written an answer (take care to set "refresh" parameter to true). When it is the case, you can then read the message length and read the message.

    A side comment: You can avoid the call to readMsgLength() . When calling readMailboxMessage() if size = 0 and mbAddress = 0, the command returns ALL bytes available.

    I would like to point something else:

    I can see that you are using "addressed commands" (this is commands containing the UID of the targeting tag).

    This is the recommended way for most Type V commands but not for Mailbox usage. When using the Mailbox, a RF command can happen at the same time as an I2C command (we call it a "collision"). When the collision happens, if you have used an addressed command, you will get a timeout (which can take up to 2 seconds!) and if you have used a non addressed command, you will get an error 01 0F. You can then retry of read the status of the Mailbox (= register REGISTER_DYN_MB_CTRL_ADDRESS) to understand what happen.

    To use a non addressed mode:

    When calling the Mailbox functions, you can pass an extra parameter called flag:

    byte flag = HIGH_DATA_RATE_MODE;

    byte[] receivedData = mST25DVTag.readMailboxMessage(0, 0, flag);

    Same thing for the other mailbox commands.

    Regards

    Olivier

    2 replies

    Olivier L
    Olivier LBest answer
    ST Employee
    June 18, 2021

    Hi,

    After writting some data in the mailbox, you should wait that the MCU writes an answer. Here, I think that you tries to read the Mailbox before that the recipient gets the time to answer. I can see that the read message length is null.

    After writing the message please use hasHostPutMsg() to monitor if the MCU has written an answer (take care to set "refresh" parameter to true). When it is the case, you can then read the message length and read the message.

    A side comment: You can avoid the call to readMsgLength() . When calling readMailboxMessage() if size = 0 and mbAddress = 0, the command returns ALL bytes available.

    I would like to point something else:

    I can see that you are using "addressed commands" (this is commands containing the UID of the targeting tag).

    This is the recommended way for most Type V commands but not for Mailbox usage. When using the Mailbox, a RF command can happen at the same time as an I2C command (we call it a "collision"). When the collision happens, if you have used an addressed command, you will get a timeout (which can take up to 2 seconds!) and if you have used a non addressed command, you will get an error 01 0F. You can then retry of read the status of the Mailbox (= register REGISTER_DYN_MB_CTRL_ADDRESS) to understand what happen.

    To use a non addressed mode:

    When calling the Mailbox functions, you can pass an extra parameter called flag:

    byte flag = HIGH_DATA_RATE_MODE;

    byte[] receivedData = mST25DVTag.readMailboxMessage(0, 0, flag);

    Same thing for the other mailbox commands.

    Regards

    Olivier

    门旭.1
    门旭.1Author
    Associate
    June 21, 2021

    Hello Olivier,

    Thanks for your answer very much! I try to use 'byte[] bytes = st25DVTag.readMailboxMessage(0, 0, HIGH_DATA_RATE_MODE);' ,it worked.

    Best wishes

    Men Xu0693W00000BbUPdQAN.png 

    Olivier L
    ST Employee
    June 28, 2021

    Hi Men Xu,

    Good, I'm glad that it works.

    Best wishes

    Olivier