CR95HF DLL x64 compatibility – is a 64-bit version available?
Hi everyone,
I’m currently working with the CR95HF and looking into using the provided DLL (CR95HF.dll) for PC-side communication.
From the documentation and software packages I understand that a DLL is provided to interface with the CR95HF demonstration board (). However, it seems this DLL was originally built for older environments and is typically installed in x32 systems, which suggests it may be a 32-bit library.
I searched the community and found a previous discussion where someone asked about x64 compatibility ( Solved: CR95HF DLL for x64 - STMicroelectronics Community ) and was provided with source code instead of a precompiled DLL.
So my questions are:
- Is there now an official x64-compatible version of the CR95HF DLL available?
- Or is the recommended approach still to request/use the source code and rebuild the DLL for x64 systems?
If rebuilding is required:
- Is there any official guidance or updated project for generating a 64-bit version?
Thanks in advance for your help!