Skip to main content
ABirj.1
Visitor II
April 13, 2021
Solved

CR95HF: Intermittent Invalid Protocol - 0x83

  • April 13, 2021
  • 1 reply
  • 631 views

Hello Folks,

We intermittently see an "invalid protocol - 0x83' error while reading data.

send_cmd 0x04 0x04 0x16 0x00 0x00 0x00

rcv_hdr 0x83 0x00

This happens intermittently and I have not been successful in reproducing the error.

Usually a restart or connect helps to resolve the error.

Any pointers on what is causing the error and how to reproduce it on a testing environment?

Best Regards,

Abhi.

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi Abhi,

    can you provide more information about the firmware being used:

    • is it based on RFAL from X-CUBE-NFC3 (or from ST25 Embedded NFC library) or is it a custom firmware implementing the commands from the datasheet?
    • do you use SPI or UART interface?
    • do you use the IRQ_OUT or SPI polling mechanism for reading response from the CR95HF?
    • on MCU side, do you use a RTOS with different tasks accessing the CR95HF?

    I suspect that sometimes the SendRcvd command is used while the protocol has been reset to field off.

    Can you connect a logic analyser on SPI (CLK, SS, MISO, MOSI) +IRQ_OUT and provide a trace?

    Rgds

    BT

    1 reply

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    April 13, 2021

    Hi Abhi,

    can you provide more information about the firmware being used:

    • is it based on RFAL from X-CUBE-NFC3 (or from ST25 Embedded NFC library) or is it a custom firmware implementing the commands from the datasheet?
    • do you use SPI or UART interface?
    • do you use the IRQ_OUT or SPI polling mechanism for reading response from the CR95HF?
    • on MCU side, do you use a RTOS with different tasks accessing the CR95HF?

    I suspect that sometimes the SendRcvd command is used while the protocol has been reset to field off.

    Can you connect a logic analyser on SPI (CLK, SS, MISO, MOSI) +IRQ_OUT and provide a trace?

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.