Skip to main content
Associate II
July 18, 2023
Solved

Crystal input for ST25R3918

  • July 18, 2023
  • 4 replies
  • 2025 views

I want to use a MEMS oscillator driving the XTI pin instead of just a crystal between XTI and XTO.  What are the specifications on the input signal?  AC coupled? Amplitude? Drive impedance? Suggested circuit for a 0V to 3.3V output oscillator?

This topic has been closed for replies.
Best answer by TedA

I don't have the option of using a standard crystal.  The chip will be used at temperatures below which crystals can be used. 

I thought that I might attenuate the oscillator output with a resistor divider and then, if necessary, capacitively couple the signal to the XTI input.

4 replies

AScha.3
Super User
July 18, 2023

so use a standard oscillator. 3v3 supply, i always put 100 ohm in clock line, to avoid reflections.

just set HSE to bypass , in Cube.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Brian TIDAL
Technical Moderator
July 18, 2023

Hi,

this post is related to Crystal input for ST25R3918 NFC reader. Your answer is likely related to STM32 MCU...

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Super User
July 19, 2023

Ooo, yes, my answer is related to STM32 MCU .

so for ST25R3918 it should be better to use just a standard crystal,

to ensure that the analogue circuits in the ST25R3918 are not disturbed.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TedAAuthor
Associate II
July 18, 2023

AScha.3

Thanks!

Ted

TedAAuthorBest answer
Associate II
July 19, 2023

I don't have the option of using a standard crystal.  The chip will be used at temperatures below which crystals can be used. 

I thought that I might attenuate the oscillator output with a resistor divider and then, if necessary, capacitively couple the signal to the XTI input.

AScha.3
Super User
July 19, 2023

exactly, this i would try also :)

AScha3_0-1689780468127.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
TedAAuthor
Associate II
July 19, 2023

AScha, Brian,

Thanks for your input.

Ted