Skip to main content
Jignesh
Associate II
July 22, 2022
Solved

Detect external NFC antenna connected to CR95HF.

  • July 22, 2022
  • 3 replies
  • 946 views

Hi,

We are using NFC reader IC: CR95HF using uart communication with our micro-controller.

We are using external antenna for antenna, Is there any way to detect NFC antenna is connected to CR95HF ?

Thank you in advance,

Jignesh Patel

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi Jignesh,

    Depending on your application, I would see several way for checking that the antenna is functional.

    1. use the Pollfield command and check the result code when the CR95HF is in the operating field of another reader. See §5.5 in the datasheet.
    2. use the TagDetection calibration procedure: when the antenna is disconnected/broken, the calibration value should be highly different from the one in nominal condition. See §5.9 in the datasheet.
    3. add a field detector (see https://www.youtube.com/watch?v=dTv4U5fotM0), switch on the field and check that the field is present.

    Rgds

    BT

    3 replies

    Brian TIDAL
    Technical Moderator
    July 22, 2022

    Hi,

    can you elaborate on your need:

    • Is it for production testing?
    • Is it for integrity testing during lifetime of your product?
    • etc.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Jignesh
    JigneshAuthor
    Associate II
    July 22, 2022

    Hi Brian TIDAL,

    It is for integration of system check during lifetime of product.

    Regards,

    Jignesh Patel

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    July 22, 2022

    Hi Jignesh,

    Depending on your application, I would see several way for checking that the antenna is functional.

    1. use the Pollfield command and check the result code when the CR95HF is in the operating field of another reader. See §5.5 in the datasheet.
    2. use the TagDetection calibration procedure: when the antenna is disconnected/broken, the calibration value should be highly different from the one in nominal condition. See §5.9 in the datasheet.
    3. add a field detector (see https://www.youtube.com/watch?v=dTv4U5fotM0), switch on the field and check that the field is present.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.