Skip to main content
Associate II
September 24, 2020
Solved

Energy harvesting and LPD: can EH still be active when the ST25 pin is put in LPD mode (the goal is to reduce the whole consumption in EH mode) ?

  • September 24, 2020
  • 2 replies
  • 933 views

..

This topic has been closed for replies.
Best answer by JL. Lebon

​Hello,

Yes, definitely. EH is completely independent of LPD, so you can have EH power when device in low power mode as well as when device has no VCC.

Best regards.

2 replies

JL. Lebon
JL. LebonBest answer
ST Employee
September 24, 2020

​Hello,

Yes, definitely. EH is completely independent of LPD, so you can have EH power when device in low power mode as well as when device has no VCC.

Best regards.

Schuyler
Associate III
June 20, 2023

@JL. Lebon 

Hi,

I need to power the STM32L4 with the energy output from the EH pin. May I ask why my LD3 power point is lit by EH pin, but the MCU does not work normally?