Skip to main content
Vmere.1
Associate III
April 20, 2022
Solved

Flash using NFC

  • April 20, 2022
  • 2 replies
  • 1276 views

On one side I have a slave MCU and other side smart phone. I have an nfc tag connected to slave MCU via I2C. Is there any way I can flash the software from smart phone to the slave MCU using NFC? Given I have some 500 Bytes EEPROM on the NFC tag.

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

ST25DV-I2C features an innovative fast transfer mode between an embedded host and an NFC phone or reader thanks to its half-duplex 256-byte buffer (mailbox). This enables use cases such as firmware update, file transfer. etc.

An end to end firmware upgrade demo from an Android phone to an ST25DV Discovery kit is available thanks to the "NFC Tap" Android app (available on GooglePlay). See UM2131 §5.2 Firmware update.

Rgds

BT

2 replies

Brian TIDAL
Technical Moderator
April 20, 2022

Hi,

which NFC tag do you use? ST25DV?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Vmere.1
Vmere.1Author
Associate III
April 21, 2022

Yes ST25DV. I have option to use others as well​

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
April 21, 2022

Hi,

ST25DV-I2C features an innovative fast transfer mode between an embedded host and an NFC phone or reader thanks to its half-duplex 256-byte buffer (mailbox). This enables use cases such as firmware update, file transfer. etc.

An end to end firmware upgrade demo from an Android phone to an ST25DV Discovery kit is available thanks to the "NFC Tap" Android app (available on GooglePlay). See UM2131 §5.2 Firmware update.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.