Skip to main content
PMK.1
Visitor II
March 22, 2022
Solved

For nfc reader can you suggest smd antenna

  • March 22, 2022
  • 1 reply
  • 929 views

..

    This topic has been closed for replies.
    Best answer by Travis Palmer

    Hello,

    there are different types of antennas.

    For all types of antennas the self resonance frequency should be above 13.56MHz. (typically between 40MHz - 120MHz). The matching network is then used to make them resonating at 13.56MHz and therefore suite able for NFC. Also the Q-factor should be in a decent range, dependent on used technology and bitrate. AN5276 is providing a good overview about important antenna parameters.

    Selecting the right antenna depends in most cases on the overall system and use-case. In an access control reader, a smd antenna could maybe also be used to read an ID1 tag, but the read range and cost might not be satisfying.

    BR Travis

    1 reply

    Travis Palmer
    Travis PalmerBest answer
    ST Employee
    April 19, 2022

    Hello,

    there are different types of antennas.

    For all types of antennas the self resonance frequency should be above 13.56MHz. (typically between 40MHz - 120MHz). The matching network is then used to make them resonating at 13.56MHz and therefore suite able for NFC. Also the Q-factor should be in a decent range, dependent on used technology and bitrate. AN5276 is providing a good overview about important antenna parameters.

    Selecting the right antenna depends in most cases on the overall system and use-case. In an access control reader, a smd antenna could maybe also be used to read an ID1 tag, but the read range and cost might not be satisfying.

    BR Travis