Skip to main content
Schuyler
Associate III
November 1, 2023
Solved

How can Sensors (SPI) be replaced?

  • November 1, 2023
  • 3 replies
  • 1134 views

Just wondering if it's possible to add an extra sensor (SPI) on the STEVAL-SMARTAG1? Can the SPI sensor be replaced to complete the acquisition?

This topic has been closed for replies.
Best answer by John TRAN

Hello there,

It is not recommended to modify the smartag board hardware. The traces and landing pads would not survive. Therefore, we prefer that you use the board AS-IS.

Best regards

 

3 replies

Michael GALIZZI
ST Employee
November 13, 2023

Hello,

On STEVAL-SMARTAG1 there is no direct access to any SPI lines. Additionally, the only sensor that uses SPI interface is the LIS2DW12: it uses a 3-wire SPI where MISO and MOSI are connected together.

Hope this help. Best regards.

Schuyler
SchuylerAuthor
Associate III
November 14, 2023

Hi @Michael GALIZZI 

Yes, the sensor's circuit is i2c communication. But I want to use three-wire SPI communication to complete the sensor acquisition, what pin should I use to complete the circuit? Doesn't the figure below mean SPI communication?GB~A`(A0D$YU`GBWB(TDIIT.png

John TRAN
John TRANBest answer
ST Employee
December 5, 2023

Hello there,

It is not recommended to modify the smartag board hardware. The traces and landing pads would not survive. Therefore, we prefer that you use the board AS-IS.

Best regards