Skip to main content
ELECL.2
Associate II
November 4, 2022
Solved

How match Molex antenna with NFC Tag ST25TA02KB-P

  • November 4, 2022
  • 3 replies
  • 1363 views

Hi,

I would like to use an existing molex antenna(1462360131) with ferrite with a NFC Tag ST25TA02KB-P.

On datasheet all tests was made with a specific antenna :

External size : 75mmx48mm

Number of truns : 4

Width of conductor : 4

Space between two conductor : 0.5mm

Value of the tuning capacitor : 50pF

Value of the coil : 2.5uH

Tuning frequency : 14.2Mhz

Molex specification :

La : 3.5uH

Ra : 5.7ohms

Ca : 3.7pF

Fra : 45.8Mhz

Rp : 10.8kohmss

Q : 52.5

    This topic has been closed for replies.
    Best answer by Henry Crane

    Hello,

    the resonant frequency of a tag antenna is given by Fr=1/(2*pi*sqrt(La_eq*Cs) where La_eq is the series equivalent inductance od the antenna at the desired tuning frequency, and Cs the series equivalent capacitance of the Tag IC.

    Our ST25TA02K tag IC has a sereis equivalent Cs= 50pF. Recommended tuning frequency for an ISO 14443-A tag is around 14MHz. The corresponding antenna inductance is La_eq_14MHz= 1/(Cs.(2.pi.13.56e6))²= 2.75µH.

    Molex antenna impedance model is Ca // (Ra + jLa.2.pi.f), where // means "in parallel to".

    The 1462360131 total impedance is 7+342.1j => 7Ohm in series with La_eq=3.89µH at 14MHz which too high, based on explanation above. The 14MHz tuning frequency can be however reached by inserting two equal series caps ( to balance the impedance on both sides of the antenna) as described below:

    0693W00000WJWcSQAX.png

    Ct1a and Ct1b are equal. CT1a=CT1b=2xCT1 where CT1 is the theoretical unbalanced capacitor is series between the antenna and the ST25TA to adjust resonant frequency:

    0693W00000WJWfHQAX.pngThe CT1 capacitor comes in series with the ST25TA02K series tuning capacitance Cs:

    0693W00000WJWgPQAX.png The new series equivalent capaciatnce seen by antenna is Ctot= (Cs.Ct1)/(Cs+Ct1). Fr=14MHz with La_eq=3.85µH means CTtot=1/(La_eq.(2.pi.14e6)²)= 34.41 pF. The corresponding CT1 value is CT=110pF. Finally, Ct1a=Ct1b=220pF.

    Another solution could be to move to the 1462360151 antenna using a parallel capacitance to increase the ST25TA02K capaciatnce wich is too llw in this case.

    feel to ask for more if necessary

    Henry Crane

    RFID/NFC Application engineer.

    3 replies

    Thomas Q.
    ST Employee
    November 10, 2022

    Hello,

    The usage of your molex antenna design with a ST25TA02KB-P tag is not straightforward because of the big gap in tuning frequency (45.8MHz vs targeted 14MHz).

    Please check document AN2866 for guidelines on NFC antenna design, and let us know if this helps in

    customization of the molex antenna to match with the ST25TA02KB-P.

    Best regards,

    Thomas

    ELECL.2
    ELECL.2Author
    Associate II
    November 18, 2022

    Thanks @Thomas Q.​ 

    Fra is not the resonant frequency.

    Attach to this reply, carateristics of this antenna :0693W00000WImOkQAL.png

    Henry Crane
    Henry CraneBest answer
    ST Employee
    November 25, 2022

    Hello,

    the resonant frequency of a tag antenna is given by Fr=1/(2*pi*sqrt(La_eq*Cs) where La_eq is the series equivalent inductance od the antenna at the desired tuning frequency, and Cs the series equivalent capacitance of the Tag IC.

    Our ST25TA02K tag IC has a sereis equivalent Cs= 50pF. Recommended tuning frequency for an ISO 14443-A tag is around 14MHz. The corresponding antenna inductance is La_eq_14MHz= 1/(Cs.(2.pi.13.56e6))²= 2.75µH.

    Molex antenna impedance model is Ca // (Ra + jLa.2.pi.f), where // means "in parallel to".

    The 1462360131 total impedance is 7+342.1j => 7Ohm in series with La_eq=3.89µH at 14MHz which too high, based on explanation above. The 14MHz tuning frequency can be however reached by inserting two equal series caps ( to balance the impedance on both sides of the antenna) as described below:

    0693W00000WJWcSQAX.png

    Ct1a and Ct1b are equal. CT1a=CT1b=2xCT1 where CT1 is the theoretical unbalanced capacitor is series between the antenna and the ST25TA to adjust resonant frequency:

    0693W00000WJWfHQAX.pngThe CT1 capacitor comes in series with the ST25TA02K series tuning capacitance Cs:

    0693W00000WJWgPQAX.png The new series equivalent capaciatnce seen by antenna is Ctot= (Cs.Ct1)/(Cs+Ct1). Fr=14MHz with La_eq=3.85µH means CTtot=1/(La_eq.(2.pi.14e6)²)= 34.41 pF. The corresponding CT1 value is CT=110pF. Finally, Ct1a=Ct1b=220pF.

    Another solution could be to move to the 1462360151 antenna using a parallel capacitance to increase the ST25TA02K capaciatnce wich is too llw in this case.

    feel to ask for more if necessary

    Henry Crane

    RFID/NFC Application engineer.