Skip to main content
PRena.1
Associate
February 21, 2023
Solved

How to increase the distance of my RFID antenna ?

  • February 21, 2023
  • 1 reply
  • 1045 views

Hello everyone !

I am writing to you because I cannot increase the transmission distance of my ST25RU3993-HPEV kit. I have bought the ST25ru3993-HPEV kit with two antenna, ...

I read that with the External PA I can increase the transmission distance but I can't do it. What is External PA ?

It does not work with External PA but in Internal it works but the distance remains limited.

I use the antennas from the kit and here are my settings:

0693W00000aHKeiQAG.png

This topic has been closed for replies.
Best answer by Bart Herse

Hello PRena.1

the external PA is used by default.

So you do not need to change the reader configuration for that.

In any case the external PA can be selected in the Tx Options section under PA Selection.

Cheers,

B

1 reply

Bart Herse
Bart HerseBest answer
Technical Moderator
March 1, 2023

Hello PRena.1

the external PA is used by default.

So you do not need to change the reader configuration for that.

In any case the external PA can be selected in the Tx Options section under PA Selection.

Cheers,

B