How to measure antenna parameters according to an4974 with NanoVNA
I have designed RFID and I am now trying to deternine the antenna parameters by following
AN4974 Antenna matching for ST25R3911B/ST25R391x devices
I have bought NanoVNA-H4 for doing the measurements.
But what confuses me is how to connect the RFID antenna.
The instructions says:
1. Set the measurement mode of the network analyzer to S11 reflection measurement
2. Use the Smith chart format (R + jX) to display the impedance curve
.
.
.
Connect the cable of the network analyzer at the antenna ends
NanoVNA-H4 has two channels S11 and S21. My PCB has a differential antenna based on this antenna design:
Then I am not sure how I shall connect the two antenna ends to my RFID. I have cut a coax cable and soldered on my PCB:
.
If I connect one end to S11 and another end to 21 of NanoVNA I get resonable values of
@1 MHz
Serie inductuance = 1.13 uH
@40.543 MHz
Parallel resistance 2.01 KOhm
Self resonance 40.543 MHz
But
DC serie resistance @ 1 MHz get 49.980 Ohm (in the documention it should be around 394 mOhm)
If I instead use S21 to measure I get DC serie resistance = 230 mOhm which seem realistic.
If only solder on cable on one end of RFID antenna, I get two resosance frequencies (around 65 and 71 MHz) and Smith chart does not look like expected.
DC serie resistance get 1.5 Ohm
So this seems wrong.
Need some help understand how this shall be done.