Skip to main content
Donatz
Associate
September 29, 2021
Solved

How to Measure RSSI using "ST25R3916_Discovery_GUI"?

  • September 29, 2021
  • 2 replies
  • 1365 views

Hi...

Good day!

I am evaluating ST25R3916-DISCO board, particularly RSSI related measurements.

The DISCO board itself displays RSSI measurement as show in the image below.

0693W00000FAkcLQAT.jpg 

However using the "ST25R3916 Discovery GUI.ver1.2",

although antenna output can be measurement as shown below...

0693W00000FAkd9QAD.jpgI cannot find RSSI measurement.

Q1 - Is RSSI measurement not included in the "ST25R3916 Discovery GUI.ver1.2 PC App?

Q2 - Could someone provide me the source code of the "ST25R3916 Discovery GUI.ver1.2 PC App?

Hoping for someone's support.

Regards,

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi Donatz,

ad Q1:

APIs to retrieve the RSSI are available - please refer to rfalGetTransceiveRSSI() which you can call after a transceive which has received a single answer to retrieve the signal strength indicator. We experimented also with adding in the GUI to the polling tab but it has a negative impact on the GUI (reactiveness and requires additional commands sent to some of the cards).

ad Q2:

Did you see the available demos which are using the provided DLL to communicate with the board? What do you want to achieve? Unfortunately RSSI is not exported on the DLL interface.

Regards, Ulysses

2 replies

Ulysses HERNIOSUS
Technical Moderator
September 29, 2021

Hi Donatz,

ad Q1:

APIs to retrieve the RSSI are available - please refer to rfalGetTransceiveRSSI() which you can call after a transceive which has received a single answer to retrieve the signal strength indicator. We experimented also with adding in the GUI to the polling tab but it has a negative impact on the GUI (reactiveness and requires additional commands sent to some of the cards).

ad Q2:

Did you see the available demos which are using the provided DLL to communicate with the board? What do you want to achieve? Unfortunately RSSI is not exported on the DLL interface.

Regards, Ulysses

Donatz
DonatzAuthor
Associate
September 29, 2021

Hi Ulysses,

Thanks for the swift response.

Your response in the DM answers it all.

Regards,

Donatz