Skip to main content
Schuyler
Associate III
September 16, 2023
Solved

How to use the captured energy to power the MCU (L476)?

  • September 16, 2023
  • 1 reply
  • 905 views

I should make an application with NFC where the entire circuit is powered by energy harvesting.
For this reason I thought of using the ST25DV and I have already purchased the X-NUCLEO-NFC07A1 and X-NUCLEO-STM32L476RG.

I have successfully obtained the energy harvesting of the antenna and can light the LED, now I want to use the energy of the antenna to wake up the MCU (L476), what do I need to do?

I have tried to connect VCC with EH pin, but L4 is not waking up, what should I do to power the antenna to the MCU (L476) instead of the ST-LINK USB

This topic has been closed for replies.

1 reply

Berenice BENVEGUDA
Technical Moderator
September 26, 2023