Skip to main content
Associate III
March 7, 2024
Solved

I have a product already developed using the M24LR64ER

  • March 7, 2024
  • 1 reply
  • 3579 views

I have a product already developed using the M24LR64ER and I need to read and write using an IPhone 14 with IOS 17, would it be possible to read and write using Swift's "import CoreNFC"?

This topic has been closed for replies.
Best answer by victor laraison

hi Greidimar,
I'm in charge of developing the iOS NFC Tap application for ST25 and M24LR tags in STMicro. 
Regarding M24LR64, they are not supported by coreNFC. It does not allow you to put the “protocol_extension_flag” necessary for the M24LR16 and M24LR64. So it is not possible to use these two versions with an iPhone (and so, whatever is the iOS NFC application used). 
I encourage you to switch on ST25DV64 tags.
Sorry for inconvenience. 
Br,

 

1 reply

victor laraison
victor laraisonBest answer
ST Employee
March 14, 2024

hi Greidimar,
I'm in charge of developing the iOS NFC Tap application for ST25 and M24LR tags in STMicro. 
Regarding M24LR64, they are not supported by coreNFC. It does not allow you to put the “protocol_extension_flag” necessary for the M24LR16 and M24LR64. So it is not possible to use these two versions with an iPhone (and so, whatever is the iOS NFC application used). 
I encourage you to switch on ST25DV64 tags.
Sorry for inconvenience. 
Br,