Skip to main content
GPaiv.1
Associate III
June 23, 2021
Solved

Is it possible to Unlock an RFID TAG ?

  • June 23, 2021
  • 1 reply
  • 4415 views

I use the standard function " STUHFL_T_RET_CODE Gen2_Lock(STUHFL_T_Gen2_Lock *lockData) " to Lock a Tag, But now I wanted to unlock the same Tag and following the standards information in Gen2 protocol Like the pictures below, I try using the same function but with a different "mask" but don't obtain a successful.

Is It possible to Unlock a Tag? Can you send a Mask to Unlock all Fields in one Tag?

Mask to Lock: FFFFFh.

Mask to Unlock: FFC0h.

https://www.gs1.org/sites/default/files/docs/epc/Gen2_Protocol_Standard.pdf

0693W00000BbqD0QAJ.png 

0693W00000BbqCqQAJ.png

This topic has been closed for replies.
Best answer by Bart Herse

Dear GPaiv.1,

looking at the lock mask you was using it seems that all memory banks have been permalocked.

As defined in the corresponding standards:

Permalock or permalocked:

A memory location whose lock status is unchangeable (i.e. the memory location is permanently locked or permanently unlocked).

Therefore unlocking is not possible anymore.

Note that your unlock mask is missing a nibble.

Note as well that in our lock function the mask information stretches over 3 bytes - maskAction[0:2]

The 20 bit mask payload is stored as shown below

maskAction[0]: Bit 19 - Bit 12

maskAction[1]: Bit 11 - Bit 4

maskAction[2]: Bit 3 - Bit 0

For maskAction[2] the lower nibble is not used: maskAction[2] & 0xf0

I hope this information is helpful.

Cheers,

B

1 reply

Bart Herse
Bart HerseBest answer
Technical Moderator
June 30, 2021

Dear GPaiv.1,

looking at the lock mask you was using it seems that all memory banks have been permalocked.

As defined in the corresponding standards:

Permalock or permalocked:

A memory location whose lock status is unchangeable (i.e. the memory location is permanently locked or permanently unlocked).

Therefore unlocking is not possible anymore.

Note that your unlock mask is missing a nibble.

Note as well that in our lock function the mask information stretches over 3 bytes - maskAction[0:2]

The 20 bit mask payload is stored as shown below

maskAction[0]: Bit 19 - Bit 12

maskAction[1]: Bit 11 - Bit 4

maskAction[2]: Bit 3 - Bit 0

For maskAction[2] the lower nibble is not used: maskAction[2] & 0xf0

I hope this information is helpful.

Cheers,

B

GPaiv.1
GPaiv.1Author
Associate III
June 30, 2021

Dear Bart,

Thanks so much, for your answer.

You help a lot, I could saw now, where are my mistake.

I'm written the wrong mask.