Skip to main content
Lakshmikanth
Associate II
January 5, 2022
Solved

Is there a provision to read temperature sensor value using SDK of ST25RU3993-EVAL board?

  • January 5, 2022
  • 1 reply
  • 611 views

Using ST25RU3993, I was able to get only the On-chip RSSI value and EPC,PC values.

Is reading the temperature sensor value, implemented in the SDK?

If NO, How can i implement it??

The temperature Sensor which I am using is "RFM3200-AFR"(Gen2 compatible).

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi,

I guess this is the same request as st25ru3993eval-access-memory-bank-of-temperature-sensor.

We have all the required information and colleague of mine will provide an answer after this holiday period.

No need to double post.

Regards, Ulysses

1 reply

Ulysses HERNIOSUS
Technical Moderator
January 5, 2022

Hi,

I guess this is the same request as st25ru3993eval-access-memory-bank-of-temperature-sensor.

We have all the required information and colleague of mine will provide an answer after this holiday period.

No need to double post.

Regards, Ulysses