Skip to main content
Associate III
January 15, 2024
Solved

NFC ndef format

  • January 15, 2024
  • 3 replies
  • 4094 views

Hi,

I have a use case where I need to read and write to an NFC tag. The read and write operation will always be done by an MCU (via st25R) and not by any other device (eg:- android device).

Should I use the NDEF format for the data in this case ? What is the advantage of using NDEF ?

 

 

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi Luke_abc,

 

The main advantage of NDEF is interoperability by giving semantic to the data. Android and Apple iPhones will read nowadays NDEF messages automatically. Android phones will know how to interpret most of the data contained in NDEF. iPhone will automatically open a few types of NDEF messages.

If you are using only one type of tag and only some proprietary data then probably no need to use NDEF, just make sure that your data is not by mistake interpreted as NDEF.

If you are using various different tags then it may become interesting to at least NFC Forum capability containers and maybe put proprietary TLVs into the NDEF file or use some mime-types. This helps you to manage different memory layouts, memory access etc. for most memory tags.

I hope this gives you some ideas what to consider.

BR, Ulysses

3 replies

Brian TIDAL
Technical Moderator
January 15, 2024

Hi,

NDEF (NFC Data Exchange Format) is a standardized message format used by NFC (Near Field Communication) devices to exchange data. The advantage of using NDEF over writing raw data on a tag is that NDEF provides a standardized way of formatting and organizing data, making it easier for different devices to read and interpret the data on the tag.

For the use case you have described, I believe there is not real advantage of using NDEF.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ulysses HERNIOSUS
Technical Moderator
January 15, 2024

Hi Luke_abc,

 

The main advantage of NDEF is interoperability by giving semantic to the data. Android and Apple iPhones will read nowadays NDEF messages automatically. Android phones will know how to interpret most of the data contained in NDEF. iPhone will automatically open a few types of NDEF messages.

If you are using only one type of tag and only some proprietary data then probably no need to use NDEF, just make sure that your data is not by mistake interpreted as NDEF.

If you are using various different tags then it may become interesting to at least NFC Forum capability containers and maybe put proprietary TLVs into the NDEF file or use some mime-types. This helps you to manage different memory layouts, memory access etc. for most memory tags.

I hope this gives you some ideas what to consider.

BR, Ulysses

Luke_abcAuthor
Associate III
January 16, 2024

Thanks @Ulysses HERNIOSUS  and @Brian TIDAL