Skip to main content
Visitor II
September 11, 2023
Solved

NFC product

  • September 11, 2023
  • 2 replies
  • 3421 views

Hello, does Android phone can serve as the NFC reader and support Fast Transfer Mode(FTM) in this diagram? If yes, what is the speed?Is FTM unique to ST NFC tag products?

xhli_0-1694426213176.png

Thanks!

This topic has been closed for replies.
Best answer by JL. Lebon

Hello xhli, 

As of today, almost all phones support NFC and they can act as NFC readers.

Concerning FTM specifically, it is perfectly possible to use it with Android (and iOS as well).
FTM is using custom RF commands, but Android provides all the necessary APIs to send and receive custom RF commands, so no problem.
The speed of FTM, with a ST25DV, is limited to 26kb/s (this is the maximum data-rate supported by smartphones in ISO15693/NFC_V).

Best regards.

2 replies

Issamos
Lead III
September 11, 2023

Hello @xhli 

Not all android phone. You should look for an android phone that support NFC communication.

Best regards.

II

JL. Lebon
JL. LebonBest answer
ST Employee
September 26, 2023

Hello xhli, 

As of today, almost all phones support NFC and they can act as NFC readers.

Concerning FTM specifically, it is perfectly possible to use it with Android (and iOS as well).
FTM is using custom RF commands, but Android provides all the necessary APIs to send and receive custom RF commands, so no problem.
The speed of FTM, with a ST25DV, is limited to 26kb/s (this is the maximum data-rate supported by smartphones in ISO15693/NFC_V).

Best regards.