Skip to main content
salugu
Associate
August 4, 2023
Solved

no response interrupt keep on triggering continuously

  • August 4, 2023
  • 2 replies
  • 3118 views

salugu_0-1691122095212.png

no response interrupt keep on triggering continuously after some time. please help in knowing the reason for this scenario.st25r3911b ic we are using and tag we are using st25tv

 

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi salugu, 

the demos as is are running and reading NFC-V tags. So the default delivered binaries should work, do they? Did you port it to a different MCU? Any other changes? In case this happens only after porting - please provide logic analyzer traces.

The no response interrupt is normal when there is no tag. Even in case the tag is there this error may still happen depending on the command sent.

BR, Ulysses 

 

2 replies

ChintaN1
Associate III
August 4, 2023

Hello Salugu,

Can you please provide more information regarding the application and configuration?

Thanks & Regards,

Chintan Patel

salugu
saluguAuthor
Associate
August 5, 2023

we are using the example code. We would like read NFC-V type tag with ISO15693.please find the attached screen shot.

salugu_0-1691217039803.png

 

Ulysses HERNIOSUS
Technical Moderator
August 7, 2023

Hi salugu, 

the demos as is are running and reading NFC-V tags. So the default delivered binaries should work, do they? Did you port it to a different MCU? Any other changes? In case this happens only after porting - please provide logic analyzer traces.

The no response interrupt is normal when there is no tag. Even in case the tag is there this error may still happen depending on the command sent.

BR, Ulysses 

 

salugu
saluguAuthor
Associate
August 5, 2023

salugu_1-1691217725772.png

this error keep on triggering even after tag is removed