NUCLEO-F401 to read ST25TV UID
Hi ST Community
I have a ST25TV tag,The UID is E0 02 08 03 8F 65 C9 F5(8bytes)
I use the board of NUCLE0-NFC08A1 and the demo in NFC6 generated by Cube MX.
I can read the relevant information of the card through the SPI provided in the demo and than print the UID of the card to the serial port(Figure1),
but I am unable to see the waveform related to the tag's UID on the logic analyzer. Could it be because the UID is encoded during transmission?
I cannot find the corresponding UID in the waveform diagram.
How can I obtain the UID by analyzing the waveform?
Figure1:

FIFO data:

waveform: