Skip to main content
Associate II
November 11, 2024
Solved

Problem with NFC-ST25R95 tag detection

  • November 11, 2024
  • 2 replies
  • 1733 views

Hello,

I'm using it with a custom board. I'm facing problem with switches the ST25R95 into low power consumption mode

When I send Calibrate command, it can work and return 0x78.

But if I send another command like wake up in IRQ_IN(07 0E 08 01 00 38 00 18 00 00 60 00 00 00 00 00) or tag detection(>0x07 0E 0A 21 00 79 01 18 00 20 60 60 70 80 3F 08),ST25R95 return me just 0xFD,

When I set it to wake up when timeout(0x07 0E 01 21 00 38 00 18 00 60 60 00 00 00 00 08) ,it return me {0x00,0x01,0x01},it is correct.

And I observed that after I sent (0x07 0E 0A  A1 00 F8 01 18 00 00 60 60 00 00 3F 01 ) to calibrated the DacDataRef,ST25R95 entered idle mode because there was not any reaction when I placed the tag on top of the antenna.

I also wanna know that what will I get from  IRQ_OUT when  I send command like wake up from tag detection,dose any reaction with IRQ_OUT as soon as I place the tag on top of the antenna?

Kindly help me out.

 

 

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

Can you describe more precisely the hardware environment used? In particular the custom board: is it using a X-NUCLEO-NFC03A1, or another ST board or is it a full custom design? (feel free to provide a picture of it). If a full custom design is being used, make sure that  Application Note AN5248 has been properly followed to have a proper matching circuit

"When I send Calibrate command, it can work and return 0x78." The ST25R95 commands set does not include a Calibrate command. Can you provide more information about this "Calibrate" command? Regarding the return if this "Calibrate" command, do you mean that the result of the calibration process is 0x78?

"But if I send another command like wake up in IRQ_IN(07 0E 08 01 00 38 00 18 00 00 60 00 00 00 00 00) or tag detection(>0x07 0E 0A 21 00 79 01 18 00 20 60 60 70 80 3F 08),ST25R95 return me just 0xFD" 0xFD is not a return code. Can you connect a logic analyzer on SPI (CLK, MISO, MOSI, CS) + IRQ_IN + IRQ_OUT and send us the trace?

"I also wanna know that what will I get from  IRQ_OUT when  I send command like wake up from tag detection,dose any reaction with IRQ_OUT as soon as I place the tag on top of the antenna?" This depends on the parameter of the IDLE command in particular the <WUPeriod>. Once a tag has been detected, the IRQ_OUT signals that the response from the IDLE command can be read.

Rgds

BT

 

 

2 replies

EyzeryongAuthor
Associate II
November 11, 2024

I also do the calibration with tag nearby, the result is almost same as open-air calibration:0x78

Brian TIDAL
Technical Moderator
November 11, 2024

HI,

can you confirm that your application relies on IRQ_OUT before reading the answer to the Idle command (see ST25R95 datasheet §5.9 "In low power consumption mode the device does not support SPI poll mechanism. Application has to rely on IRQ_OUT before reading the answer to the Idle command.")?

Also, I would recommend to base you application on top of the RF Abstraction Layer library provided in the ST25 embedded NFC library. It provides demos application and supports the tag detection.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
EyzeryongAuthor
Associate II
November 12, 2024

Hi,

I can confirm my application relies on IRQ_OUT before reading the answer to the Idle command

But I didn't use ST25 embedded NFC library.I try to understand the code in the library ,It needs me to spend some time, so can you help me explain my question above first?

thanks.

Brian TIDAL
Technical Moderator
November 15, 2024

Hi,

this is a normal behavior.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.