Skip to main content
STHOR.1
Associate
May 27, 2021
Solved

Protected access with ST25R25 or CR95HF

  • May 27, 2021
  • 3 replies
  • 881 views

Dear Sir/Madame,

I'm currently using ST25R95 for a design and I have a question from my software colleagues.

Is the device capable of writing on Tags with a protected acess (by password for example)  ? 

We are using NFC TAGs Type 1.

We would like to garantee that we can read and write the memory of the tags but without the possibility to copy what we are reading.

We would like to ensure that no other reader than our can access to the memory of the tags.

Thx in advance,

Sincerely,

S.T

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi Sebastien,

    for your information, a C library for the ST25R5 is available on st.com (X-CUBE-NFC3 package). It provides a polling demo (polls for various tag technologies and displays tag UID) and NDEF demo (NDEF read and write). It is a good starting point for customer application development.

    Another information, type 1 tags are getting soon deprecated by NFC Forum. I would rather recommend to use ST25TA or ST25TV tags that support password protection features. The X-CUBE-NFC3 supports the ST25TV password protection commands

    Rgds

    BT

    3 replies

    Ulysses HERNIOSUS
    Technical Moderator
    May 27, 2021

    Hi STHOR.1,

    what you describe will require strong cryptography. Type 1 Tag according to NFC Forum spec does not implement any protection / cryptography.

    An NFC reader/writer is able to arbitrary frames. All protection etc is up to the upper software layers using the chip / our software libraries.

    Best Regards, Ulysses

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    May 27, 2021

    Hi Sebastien,

    for your information, a C library for the ST25R5 is available on st.com (X-CUBE-NFC3 package). It provides a polling demo (polls for various tag technologies and displays tag UID) and NDEF demo (NDEF read and write). It is a good starting point for customer application development.

    Another information, type 1 tags are getting soon deprecated by NFC Forum. I would rather recommend to use ST25TA or ST25TV tags that support password protection features. The X-CUBE-NFC3 supports the ST25TV password protection commands

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    STHOR.1
    STHOR.1Author
    Associate
    May 27, 2021

    Hi Ulysses and Brian,

    Thank you for your both answers.

    Regards,

    S.T.