Skip to main content
This topic has been closed for replies.
Best answer by JL. Lebon

Hello,

You can protect memory areas in read and/or write.
Protection can be either temporarily disabled by a password presentation or permanent.

To enable the data protection for a memory area, you have 4 configuration Bytes (one per possible memory area): RFA1SS, RFA2SS, RFA3SS and RFA4SS. Please refer to the chapter "5.6 Data protection" of the datasheet for the description of those configuration bytes.

You may also want to configure the memory in several areas. Each area can be individually protected. By default (factory setting), there is only one area, occupying the full memory.

Typically, if you want to protect the write access of this area (area1), you would write RFA1SS=05h. This would protect your area1 (full memory by default) in write, with password 1. In order to write into area1, you would then have to present the password 1 first (Present Password command), otherwise write would fail. Password 1 is be default all 00, but you can change it with a Write Password command.

Best regards.

1 reply

JL. Lebon
JL. LebonBest answer
ST Employee
June 20, 2023

Hello,

You can protect memory areas in read and/or write.
Protection can be either temporarily disabled by a password presentation or permanent.

To enable the data protection for a memory area, you have 4 configuration Bytes (one per possible memory area): RFA1SS, RFA2SS, RFA3SS and RFA4SS. Please refer to the chapter "5.6 Data protection" of the datasheet for the description of those configuration bytes.

You may also want to configure the memory in several areas. Each area can be individually protected. By default (factory setting), there is only one area, occupying the full memory.

Typically, if you want to protect the write access of this area (area1), you would write RFA1SS=05h. This would protect your area1 (full memory by default) in write, with password 1. In order to write into area1, you would then have to present the password 1 first (Present Password command), otherwise write would fail. Password 1 is be default all 00, but you can change it with a Write Password command.

Best regards.