Seeking NFC chip with GP input; Q's about energy harvesting and i2c
1) Does ST make an NFC tag chip that has even one general-purpose, digital input detectable by the tag reader?
2) Can a ST25DV04KC's energy harvesting really power up an 8-bit MPU long enough to take a sensor reading and write back via i2c? The MPU would need to run at 4-8MHz for a very short period of time.
3) Is this i2c interface a "slave" only, or can it read an external i2c sensor under NFC reader control?
4) Does this NFC family "play nice" w.r.t. (avoiding) collisions between, say, 4-5 other devices within the EM field, so the tag reader can read them all within approximately 100ms? (all identical ST NFC tags, of course).