Skip to main content
JHave.1
Associate
April 11, 2024
Solved

ST25 NFC Tap app issue on Android Version 14

  • April 11, 2024
  • 1 reply
  • 1326 views

We are testing the app on a newer mobile and encountered this issue:

Calling this function will cause the application to crash:

mFtmCommands = new FtmCommands(mST25DVTag);

The problem is in this procedure:

private void setMaxTransmissionSize() {
if (this.mST25DVTag != null) {
this.mMaxTransceiveSize = this.mST25DVTag.getReaderInterface().getMaxTransmitLengthInBytes();
if (this.mUseAddressedMode) {
this.mMaxTransmissionSize = Math.min(this.mMaxTransceiveSize - 12, 256);
} else {
this.mMaxTransmissionSize = Math.min(this.mMaxTransceiveSize - 4, 256);
}
}

}

specifically this line:

this.mMaxTransceiveSize = this.mST25DVTag.getReaderInterface().getMaxTransmitLengthInBytes();

If the mobile phone is close to the NFC antenna, the problem does not occur, if the phone is out of range, the application crashes.

(There is not problem on the older Android Version 9...)

This topic has been closed for replies.
Best answer by Entony

Hello and thank you for your reply. It was my mistake, I was using an old version of the app. (st25nfcApplication_V3.7.0).

Everything is okay now.

1 reply

France Berthelot
ST Employee
April 24, 2024

Hello

Thaks for the feedback.

I did some tests on several phones with different Android versions (Pixel3/Android12, Pixel 6Pro/Android14) without reproducing the issue.

The NFCTap version is (menu/About) : V3.10.0 with ST25SDK:1.10.0 (The last posted on google play)

Can you please check that you are aligned ?

I use in front of the phone a ST25 discovery MBoard MB136-A with a ST25DV04K-I and menu FTM with power plugged.

The app see the Tag and identify the board name.

I did the following:

Try to send data to Tag in several configurations, on tag and far away from tag... I have : cmd failed or No response received (according to board config) or command successful when transfer is done.

No way to reproduce.

Is it possible for you, to describe also the context on which you have the issue (steps to reproduce, phone/board/version used)?

Thanks in advance

FB

 

 

 

 

Entony
EntonyBest answer
Associate II
May 2, 2024

Hello and thank you for your reply. It was my mistake, I was using an old version of the app. (st25nfcApplication_V3.7.0).

Everything is okay now.