Associate
April 20, 2026
Question
ST25DV04 antenna connection
- April 20, 2026
- 2 replies
- 104 views
I want to add NFC functionality to an existing product. Because the PCB is made of aluminium, I can't use a PCB antenna.
On the enclosure of the product, there is a small PCB with 2 pushbuttons and some leds. My idea is to place the PCB antenna on this small PCB.
But because of space restrictions, I can't add positions to the existing connector.
My idea is to connect the antenna in parallel to the pushbuttons (see attached drawing). The GPIOs of the uP are inputs. I'm aware that the NFC does not work if a pushbutton is being pressed.
My questions are: Do you think this can work? Can the ST25DV04 take damage, if an antenna connection is shortet to GND? Can the 1K resistors remain in the circuit or do I need to replace them with 0R resisorts?