Skip to main content
Visitor II
August 28, 2025
Solved

ST25DV04K – RF password and factory reset

  • August 28, 2025
  • 2 replies
  • 321 views

Hello everyone,

I’m currently working with the ST25DV04K chip and I’ve noticed two points that are a bit confusing:

  1. There doesn’t seem to be any way to change the RF passwords via I²C.

  2. I couldn’t find any command that allows a full factory reset (including resetting the passwords).

My questions are:

  • Is this really the case, or am I missing some undocumented/hidden command?

  • If the passwords are set via I²C and cannot be changed anymore, doesn’t this risk making the device unusable in case of a configuration mistake?

  • Is there any recommended method from ST to bring the chip back to a “clean” state without replacing it?

Thanks in advance to anyone who can clarify these points.

This topic has been closed for replies.
Best answer by JL. Lebon

Hello,

Let me answer your questions one by one:

"There doesn’t seem to be any way to change the RF passwords via I²C."
-> no there is not. I2C passwords can only be changed from I2C interface and RF passwords can only be changed from RF interface.

"I couldn’t find any command that allows a full factory reset (including resetting the passwords)."
-> there is no such command. Factory reset is not possible.

"Is this really the case, or am I missing some undocumented/hidden command?"
-> your understanding is correct.

"If the passwords are set via I²C and cannot be changed anymore, doesn’t this risk making the device unusable in case of a configuration mistake?"
-> yes, if you forget your password, there is no way to recover or reset it.

"Is there any recommended method from ST to bring the chip back to a “clean” state without replacing it?"
-> If you forgot the password, there is no way to go back to clean state. That would be a serious security breach!

Best regards.

2 replies

Brian TIDAL
Technical Moderator
August 29, 2025

Hi,

do you use the ST25DV04K or the ST25DV04KC? ST25DV04K  is Not Recommended for New Design (NRND) whereas ST25DV04KC is active.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JL. Lebon
JL. LebonBest answer
ST Employee
September 1, 2025

Hello,

Let me answer your questions one by one:

"There doesn’t seem to be any way to change the RF passwords via I²C."
-> no there is not. I2C passwords can only be changed from I2C interface and RF passwords can only be changed from RF interface.

"I couldn’t find any command that allows a full factory reset (including resetting the passwords)."
-> there is no such command. Factory reset is not possible.

"Is this really the case, or am I missing some undocumented/hidden command?"
-> your understanding is correct.

"If the passwords are set via I²C and cannot be changed anymore, doesn’t this risk making the device unusable in case of a configuration mistake?"
-> yes, if you forget your password, there is no way to recover or reset it.

"Is there any recommended method from ST to bring the chip back to a “clean” state without replacing it?"
-> If you forgot the password, there is no way to go back to clean state. That would be a serious security breach!

Best regards.