ST25DV04KC GPO no interrupt output
I am implementing NFC wake-up functionality using the main controller chip STM32L433 and the ST25DV04KC. I2C writes and reads are functioning normally.
However, when the NFC field is present, the GPO pin does not output a pulse (reading the GPO register returns a value of 0x11). Using a multimeter to measure the GPO level change when the NFC field appears shows a minimal change in voltage level.
The same program works correctly on an STM32F1 development board with an ST25DV04KC NFC module (both 8-pin and 12-pin versions were tested, with the same phenomenon).
Does anyone know why this is happening?Could you provide some troubleshooting directions?This would be very helpful to me.Thank you!