ST25R Antenna Matching tool with specific antenna
- July 7, 2023
- 2 replies
- 2989 views
Hey, i am developing a RFID reader for ISO-14443-4 card with st25r3917b. The firmware is done and works with my custom MCU board connected with external RF board of STEVAL-25R3916B. However , if I switching the testboard and connect with my custom RFID board ,the reader just can not detect the card .It is obviously cause by wrong matching circuit I draw before.The antenna parameter to the Antenna matching tool is still a question for me to implement a custom antenna for the project.
Due to lacking of newwork analyzer and imformation from the antenna datasheet. Some of the parameter from the Antenna Matching tool is still missing(Target Q , Targeting Matching Z, Parallel resistance and the present box?). Should i just enter some general numbers in the blank?
In my test , there are three board , one main board only contain MCU(STM32L452CCU6), one STEVAL-25R3916B RF board and one custom st25r3917b board contain RFID antenna with cable(FXR.01.07.0100C.A). In the Antenna Matching tool , the topology is using the config [3916-single-ended-cable]