Skip to main content
Visitor II
November 26, 2024
Solved

ST25R3911 Reading T2T cards fails

  • November 26, 2024
  • 1 reply
  • 516 views

hello,

  Currently I use nfc5 demo to read T2T card, but the read often fails,The code is as follows.When NFC-A is detected, the type is 0, and the card is considered to be T2T

 

static void demoT2t(void)
{
  ReturnCode err;
  uint16_t rcvLen;
  uint8_t blockNum = 0;
  uint8_t rxBuf[16];

  err = rfalT2TPollerRead(0, rxBuf, sizeof(rxBuf), &rcvLen);
  printf("err %d\r\n", err);
  platformLog(" Read Block %d: %s %s\r\n", 0, (err != ERR_NONE) ? "FAIL" : "OK Data:", (err != ERR_NONE) ? "" : hex2Str(rxBuf, rcvLen));
}
 
LYU4662_0-1732610070536.png
LYU4662_1-1732610503510.png
LYU4662_2-1732610546453.png

These cards are detected in the code as T2T type, and there is no encryption, and I can see from the app read that the keys are all 0xFF,I wonder what went wrong, thanks

LYU4662_3-1732610814774.png

 

 

 
This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

such tags are not true T2T tags as a proprietary three pass authentication is required before memory operation. See https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/nfc0541-read-mifare-classic-1k/td-p/255197 for similar question. I would suggest to use true T2T tags such ST25TN rather that tags with proprietary authentication and ciphering which are broken since several years.

Rgds

BT

1 reply

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
November 26, 2024

Hi,

such tags are not true T2T tags as a proprietary three pass authentication is required before memory operation. See https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/nfc0541-read-mifare-classic-1k/td-p/255197 for similar question. I would suggest to use true T2T tags such ST25TN rather that tags with proprietary authentication and ciphering which are broken since several years.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.