Skip to main content
Associate
September 2, 2025
Solved

ST25R3911B Antenna Response Distance and Impedance Matching Debugging

  • September 2, 2025
  • 2 replies
  • 986 views

This is a custom-made PCB antenna board utilising the ST25R3911B chip, but I am unsure how to proceed with impedance matching debugging and parameter configuration.

Could you offer some guidance? Below are the antenna dimensions, the calculated impedance matching values, and the original impedance matching diagram. Communication is currently possible at very close range.

To increase communication distance and stability, what modifications should be made?

Jluu_0-1756802810927.png

Jluu_1-1756802820331.png

Jluu_2-1756802854425.png

 

*This post has been translated from Chinese to comply with the ST Community guidelines.

 

This topic has been closed for replies.
Best answer by Travis Palmer

Hello J-luu,

 

It is not very easily possible to tune a NFC reader without VNA.

There is a nanoVNA H4, which is quite affordable. 

Even if you use a pre-tuned 50Ohm antenna, it is recommended to check the tuning. Parasitics introduced with the layout or PCB layerstack can have very bad influence on the matching. 

One other solution is to rent a service at a university or consult an external RF design house.

BR Travis

2 replies

Ulysses HERNIOSUS
Technical Moderator
September 2, 2025
Travis Palmer
ST Employee
September 12, 2025

Hi J-luu,

 

120nH antenna inductance seems very little for a 4 turn antenna with approx.. 30 to 40mm diameter.

Could you please share a smith chart of the antenna and antenna + matching network?

What is the read range you are able to achieve and what is your desired read range?

BR Travis

J-luuAuthor
Associate
September 19, 2025

Jluu_0-1758263827265.png

Jluu_1-1758264033201.png

Jluu_2-1758264055347.png

The impedance matching network currently in use is shown in Figure 1, with STMicroelectronics' official analysis depicted in Figure 2. Compared to Figure 3, the present reading range is limited to 5 cm. How might we optimise the antenna to achieve a reading range of approximately 10 cm? Alternatively, could you provide a correctly designed circular antenna? Owing to the lack of equipment for measuring antenna parameters, we can only input calculated values for impedance matching.

 

*This post has been translated from Chinese to comply with the ST Community guidelines.

 

Travis Palmer
Travis PalmerBest answer
ST Employee
October 28, 2025

Hello J-luu,

 

It is not very easily possible to tune a NFC reader without VNA.

There is a nanoVNA H4, which is quite affordable. 

Even if you use a pre-tuned 50Ohm antenna, it is recommended to check the tuning. Parasitics introduced with the layout or PCB layerstack can have very bad influence on the matching. 

One other solution is to rent a service at a university or consult an external RF design house.

BR Travis