Skip to main content
Schuyler
Associate III
May 10, 2023
Solved

ST25R3911B-DISCO debugger connection

  • May 10, 2023
  • 1 reply
  • 787 views

I have a question, I don't know if 3911 in the image below is jtag download code or SWD.


_legacyfs_online_stmicro_images_0693W00000bjn3lQAA.png

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    P201 10-pin connector on ST253911B-DISCO is a JTAG/SWD interface to assist in software development on the onboard STM32L476RE. It can be connected to an external ST-LINK/V2 device using a 9-pin Cortex®-M adapter. See User Manual UM2042 for description of the ST253911B-DISCO and see STM32L476RE Reference manual RM0351 for details about the Single Wire/JTAG Debug Port.

    Rgds

    BT

    1 reply

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    May 10, 2023

    Hi,

    P201 10-pin connector on ST253911B-DISCO is a JTAG/SWD interface to assist in software development on the onboard STM32L476RE. It can be connected to an external ST-LINK/V2 device using a 9-pin Cortex®-M adapter. See User Manual UM2042 for description of the ST253911B-DISCO and see STM32L476RE Reference manual RM0351 for details about the Single Wire/JTAG Debug Port.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.