ST25R3911B SPI issues
Hello,
I got back to my issues from this post.
I was able to connect wires to SPI lines, and get the measurements to logic analyzer. These are the results:
Logic2 screenshot
Now i can see that the issue is the CS line, but i dont know why it is being changed to HIGH in these short pulses.
The GPIO config:
/*Configure GPIO pin : SPI1_CS_Pin */
GPIO_InitStruct.Pin = SPI1_CS_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(SPI1_CS_GPIO_Port, &GPIO_InitStruct);SPI Config:
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
And the PCB Traces:

Edited to apply source code formatting - please see How to insert source code for future reference.