ST25R3916 Adjust Regulators not completing without a tag in the field
As we've been integrating the ST25R3916 into our final hardware, there's been an issue with the Adjust Regulators command. On external supply power, the command works without any problems. On some (not all) of our battery-powered units, as tested in the field, the Adjust Regulators command never returns, so NFC is unable to initialize. The weird part is that when a tag is held inside the field during initialization, the command completes without any issues and NFC initializes. I assume this is because the tag increases impedance while it pulls power, but this should not be necessary and our system is able to handle the current. The two traces below show initialization with a tag in the field (first), and failure without a tag in the field (second). At no point does the 2.8V rail dip, so I don't see this as an issue with the power supply.
VDD_2.8 (green)
VDD_D (red)
VDD_AM (blue)
VDD_RF (yellow)


I tried with every value of RFO driver resistance, and none worked. Setting the regulated voltage manually did, but that's not a solution that we can use going forward. Is there something I'm missing here to ensure this command completes successfully? The application is for NFC-A only, so the VDD_AM jumping around makes me wonder if there's amplitude modulation happening that shouldn't be, and messing up the initialization somehow.