ST25R3916B not detecting tags
- February 10, 2023
- 4 replies
- 1280 views
Hello,
I ported the porting example to a different processor. The self tests are enabled and initialization passes. However I'm not able to read a tag. Logic captures (Salae) are attached. I've verified that I'm receiving interrupts and processing them. I also tested this hardware with an externally NUCLEO-L476RG board and off the shelf firmware and it could read the tags fine. Tags are very close to the antenna, within 1cm.
I noticed that when a 14443 tag is present, the number of interrupts increase, from about 15 per second without a tag, to 20 per second with a tag. But it never outputs the UUID of the tag itself. In the captures I observed that the interrupt gets serviced in about 20uSec.
Other than the platform files I tried to duplicate the demo firmware as closely as possible, leaving all the technologies enabled, not using ST25R_COM_SINGLETXRX, etc.
Thanks,
Derek