Skip to main content
Associate II
October 20, 2023
Solved

ST25R3916B RF power output

  • October 20, 2023
  • 1 reply
  • 1917 views

Hi, it's not clear the deliverable power of the ST25R3916B. it seems 1.6W in balance output configuration. On the datasheet is written only that there is a dynamic power output, on the first page then no more other information, and there are no registers about the output power it seems..

I have to do a connection P2P between 2 eval NUCLEO-NFC08A1, but i get only 9cm of maximum distance range. it's a poor result for 1.6W...

is there the possibility to control manually the power output?

how is it possible to increse the distance range in P2P mode (without changing the antenna)?

i'm waiting your reply soon

thanks

Logantenna

This topic has been closed for replies.
Best answer by pablog

Hello,

Keeping in mind that the NFC technology is intended for short range/security communications and that it has been developed with a range not greater than 10cm, 9cm seems very good range to me.

Q: Is there the possibility to control manually the power output?
A: If you have it set as a Tag, I believe you can't change the power.  But if you use it as a Read/Write, then you can.  There is a register somewhere.

Q: How is it possible to increase the distance range in P2P mode (without changing the antenna)?
A: You can change the matching of the NFC antenna.  Check Figure 4 on the App Note AN4974.



    

1 reply

pablogBest answer
Associate
January 18, 2024

Hello,

Keeping in mind that the NFC technology is intended for short range/security communications and that it has been developed with a range not greater than 10cm, 9cm seems very good range to me.

Q: Is there the possibility to control manually the power output?
A: If you have it set as a Tag, I believe you can't change the power.  But if you use it as a Read/Write, then you can.  There is a register somewhere.

Q: How is it possible to increase the distance range in P2P mode (without changing the antenna)?
A: You can change the matching of the NFC antenna.  Check Figure 4 on the App Note AN4974.



    

Associate II
January 19, 2024

Thanks for the reply