Skip to main content
LHing.1
Associate
November 9, 2021
Solved

ST25R3917 as direct replacement in a ST25R3916 project

  • November 9, 2021
  • 3 replies
  • 943 views

Can the ST25R3917 be used as direct replacement in a ST25R3916 project based on X-NUCLEO-NFC06A1, or do I need to change anything in the code?

I am aware that some hardware features aren't available.

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi LHing.1,

yes it can be used as a direct replacement. If you have code running on ST25R3916 which is not using any features not available on the 3917 then it will run out of the box on ST25R3917.

Best Regards, Ulysses

3 replies

Brian TIDAL
Technical Moderator
November 9, 2021

Hi,

is it X-NUCLEO-NFC05A1 (ST25R3911B based) or X-NUCLEO-NFC06A1 (ST25R3916 based)?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LHing.1
LHing.1Author
Associate
November 9, 2021

It is X-NUCLEO-NFC06A1 based, I'll fix the typo.

Ulysses HERNIOSUS
Technical Moderator
November 9, 2021

Hi LHing.1,

yes it can be used as a direct replacement. If you have code running on ST25R3916 which is not using any features not available on the 3917 then it will run out of the box on ST25R3917.

Best Regards, Ulysses