ST25R3917 not receiving 9000 answer to APDU (AID)
Hello,
We are trying to implement the isodep functionality in one of our developments with the ST25R3917, acting as reader/PCD. We have implemented the libraries included in the STSW-ST25R018 firmware (https://www.st.com/en/embedded-software/stsw-st25r018.html) .
By other side, we have an Android App with a customized AID, already tested and working. It answers with 0x9000 when it receives the APDU containing the AID previosuly configurated. We have checked it with the ST25R3916 Discovery Board with the firmware version 1.4.3 (see following picture)

However, when we try to communicate with the App, using the libraries that I mentioned before, the answer to the APDU containing the AID (00 A4 04 00 07 XX XX XX XX XX XX XX) is 0xF208, which seems to be a S-Block message indicating the WTX period. In the libraries the behaviour to this answer is to send the same message received to the PICC (our smartphone in this case), until the PCD (our device) receives the right answer (0x9000). But when the ST25R3917 sends this message, it recives nothing from the PICC.
I have checked that all the previous steps have been completed succesfully:
-The field is on
-The answer to the WUPA command is 0x0400
-The answer to the RATS command is 0x0578804400 (TL: 0x05, T0: 0x78, TA: 0x80, TB: 0x44, TC: 0x00)
-The APDU is sent correctly with one pcb byte at the beginning (02 00 A4 04 00 07 XX XX XX XX XX XX XX)
Do you know what could be the problem?
Thank you in advance.
Regards,