Skip to main content
Explorer II
February 6, 2024
Solved

STEVAL-25R3916B 66 x 66 mm 2 turns antenna data

  • February 6, 2024
  • 1 reply
  • 816 views

Hi,

I am new to NFC therefore using the kit as a starting point. I learnt that we can use the following tools to design the antenna:-

https://eds.st.com/antenna/#/

 

Question 1

If I am using the  tool (https://eds.st.com/antenna/#/) to help design the antenna and to find the right capacitance for the matching network,

what sort of data(the field marked with ?) should I enter on the page as shown below?

Geometry
Turns: 2
Antenna Length: ? mm
Antenna Width: ? mm

Conductor
Width: ? mm
Spacing: ? mm
Thickness: ? um

Substrate
Thickness: ? mm
RElative Electrical Permittivity: ?

Resonant freq: 13.56MHz

 

 

Question 2: STEVAL-25R3916B_Antenna.png

Can you provide me with the value of the antenna inductance?

 

Thanks in advance!!!

 

Best Regards,

Cindy

 

 

 

 

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi Cindy,

please study AN5276 and AN5322.

BR, Ulysses

1 reply

Ulysses HERNIOSUS
Technical Moderator
February 7, 2024

Hi Cindy,

please study AN5276 and AN5322.

BR, Ulysses