Skip to main content
Senior
November 7, 2023
Solved

Using AAT on NFC08a1

  • November 7, 2023
  • 2 replies
  • 2156 views

Hello everyone,
I am using an NFC08A1 for my project and I would like to use the AAT. I roughly understand what happens in the AAT algorithm. However, I don't get any noticeable improvement when I apply it. The range in particular remains almost the same.

An external antenna is used in the project and I would like to achieve optimum performance. Which default values do I have to change in the algorithm to achieve this? And when does it make sense to call the AAT? Later I want to switch between two readers. Is it necessery to call the function everytime I change the reader or is it possible to store the best configuration. 

Rgds

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi,

two remarks here:

  1. Did you disable the setting of AAT registers from analog config? Per default these are overwriting any tuned values....
  2. On a well tuned board like the NFC08 without a strong detuning element there is likely not much of an effect. You can try to put a metal plate close and then you may see a difference of re-tuned vs un-tuned antenna. But don't expect a boost of multiple centimeters!

BR, Ulysses

2 replies

Ulysses HERNIOSUS
Technical Moderator
November 7, 2023

Hi,

two remarks here:

  1. Did you disable the setting of AAT registers from analog config? Per default these are overwriting any tuned values....
  2. On a well tuned board like the NFC08 without a strong detuning element there is likely not much of an effect. You can try to put a metal plate close and then you may see a difference of re-tuned vs un-tuned antenna. But don't expect a boost of multiple centimeters!

BR, Ulysses

CT-55555Author
Senior
November 8, 2023

Hi,

1. Did you mean this part of the rfal_analogConfigTbl.h: 

CT55555_0-1699429928156.png

if not please let me know. 

2. I connected a external Antenna to the board using normal wires. The distance between the antenna and the board is now about 100 cm. I also placed different metall objects near the antenna. I think these are strong detuning elements. 

Rgds 

 

Ulysses HERNIOSUS
Technical Moderator
November 8, 2023

Hi,

ad 1) Yes, it is about these registers. Critical for you is not the setting in CHIP_INIT but the other settings in POLL_COMMON and LISTEN_*. I think in the GUI we are providing analog configs for playing with the AAT (which don't have these settings) - also mentioned in the AAT appnote.

ad 2. Are you having 1m in differential mode. Not sure how well this can work. Maybe @Travis Palmer can comment on this.

 

BR, Ulysses

Roger SHIVELY
ST Employee
November 8, 2023

Hello @CT-55555 ,

There has been a case created to resolve this question and we will be reaching out to you directly.

Regards,
Roger