Skip to main content
LM.2
Associate II
March 24, 2022
Solved

x-cube-nfc3 UART issues, passing initialisation but not detecting NFC tags.

  • March 24, 2022
  • 1 reply
  • 1298 views

Hey,

I have been using the x-cube-nfc3 demo for Nucleo-l496ZG 144 pin board along with a CR95HF. In SPI mode I can successfully initialise and read the ID from NFC tags. I attempted to change to UART mode by adding

#define ST25R95_INTERFACE_UART 1

to platform.h. I also changed the macros in platform.h from huart1 to huart3 because it saved soldering of additional headers.

With these modifications the device initialises successfully over UART however I cannot get it to detect any NFC tags.

Are there any more modifications needed?

This topic has been closed for replies.
Best answer by Brian TIDAL

HI,

the SSI_0 (signal D9 on CN5 connector of the X-NUCLEO-NFC03A1 board) has to be set to low (see table 4 of the CR95HF datasheet) in order to properly select the UART interface during the startup sequence (see § 3.2 of the datasheet). Make sure the GPIO connected to SSI_0 is set to low in your configuration.

On Software side, the UART interrupt has to be enabled and the HAL_UART_TxCpltCallback, HAL_UART_RxCpltCallback and HAL_UART_ErrorCallback have to be populated with  st25r95UartTxCpltCallback (resp. st25r95UartRxCpltCallback, st25r95UartErrorCallback). See https://community.st.com/s/question/0D50X0000B7YwL7SQK/how-to-use-uart-interface-instead-of-spi-with-xnucleonfc03a1-and-xcubenfc3-polling-demo for further details (it also provides a demo package based on X-CUBE-NFC3 2.0.0 that should help).

st25r95Initialize() does 5 attempts to send an echo command with UART TX/RX in blocking mode. If the UART communication fails (no reply to echo command), the st25r95Initialize returns ERR_SYSTEM. If it returns ERR_NONE, it means your UART communication is OK. Then further communication uses UART TX/RX with interrupt mode. If this part is failing, make sure to enable the UART interrupt and to populate the callbacks.

Note: You can enable ST25R95_DEBUG to have some extra traces

Rgds

BT

1 reply

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
March 24, 2022

HI,

the SSI_0 (signal D9 on CN5 connector of the X-NUCLEO-NFC03A1 board) has to be set to low (see table 4 of the CR95HF datasheet) in order to properly select the UART interface during the startup sequence (see § 3.2 of the datasheet). Make sure the GPIO connected to SSI_0 is set to low in your configuration.

On Software side, the UART interrupt has to be enabled and the HAL_UART_TxCpltCallback, HAL_UART_RxCpltCallback and HAL_UART_ErrorCallback have to be populated with  st25r95UartTxCpltCallback (resp. st25r95UartRxCpltCallback, st25r95UartErrorCallback). See https://community.st.com/s/question/0D50X0000B7YwL7SQK/how-to-use-uart-interface-instead-of-spi-with-xnucleonfc03a1-and-xcubenfc3-polling-demo for further details (it also provides a demo package based on X-CUBE-NFC3 2.0.0 that should help).

st25r95Initialize() does 5 attempts to send an echo command with UART TX/RX in blocking mode. If the UART communication fails (no reply to echo command), the st25r95Initialize returns ERR_SYSTEM. If it returns ERR_NONE, it means your UART communication is OK. Then further communication uses UART TX/RX with interrupt mode. If this part is failing, make sure to enable the UART interrupt and to populate the callbacks.

Note: You can enable ST25R95_DEBUG to have some extra traces

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LM.2
LM.2Author
Associate II
March 25, 2022

Thank you Brian

I didn't realise that it was swapping from polling to interrupt mode. Adding the interrupt callbacks fixed all of my issues.