Skip to main content
Schuyler
Associate III
March 10, 2023
Solved

X-CUBE_NFC7: no NDEF seen by the phone

  • March 10, 2023
  • 4 replies
  • 1275 views

I used the I2C example in X-CUBE-NFC7 to write "hello the world" and wanted to read the data from the phone, but according to the above code the phone does not show any NDEF information, what should I do?

/* USER CODE BEGIN Header */

/**

 ******************************************************************************

 * @file      : main.c

 * @brief     : Main program body

 ******************************************************************************

 * @attention

 *

 * Copyright (c) 2021 STMicroelectronics.

 * All rights reserved.

 *

 * This software is licensed under terms that can be found in the LICENSE file

 * in the root directory of this software component.

 * If no LICENSE file comes with this software, it is provided AS-IS.

 *

 ******************************************************************************

 */

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "main.h"

#include "app_nfc7.h"

#include "nfc07a1_nfctag.h"

#include <stdio.h>

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

#define NFC_BUFFER_SIZE 64

/* NFC数�?�读写缓冲区 */

#define NFC_BUFFER_SIZE 64

uint8_t nfc_data[NFC_BUFFER_SIZE];

/* USER CODE END 0 */

/**

 * @brief The application entry point.

 * @retval int

 */

int main(void)

{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_NFC7_Init();

 /* USER CODE BEGIN 2 */

 /* �?�NFC标签中写入数�?� */

  uint8_t write_data[] = "hello the world";

  NFC07A1_NFCTAG_WriteData(0, write_data, 0, sizeof(write_data));

  /* 从NFC标签中读�?�数�?� */

  uint16_t read_size = 0;

 read_size = NFC07A1_NFCTAG_ReadData(0, nfc_data, 0, NFC_BUFFER_SIZE);

  /* 打�?�读�?�到的数�?� */

  printf("Read from NFC tag: %s\n",nfc_data);

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

 MX_NFC7_Process();

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

/**

 * @brief System Clock Configuration

 * @retval None

 */

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage

 */

 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)

 {

  Error_Handler();

 }

 /** Initializes the RCC Oscillators according to the specified parameters

 * in the RCC_OscInitTypeDef structure.

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

 RCC_OscInitStruct.HSIState = RCC_HSI_ON;

 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

 RCC_OscInitStruct.PLL.PLLM = 1;

 RCC_OscInitStruct.PLL.PLLN = 10;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;

 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;

 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

 /** Initializes the CPU, AHB and APB buses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

               |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)

 {

  Error_Handler();

 }

}

/**

 * @brief GPIO Initialization Function

 * @param None

 * @retval None

 */

static void MX_GPIO_Init(void)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */

 __HAL_RCC_GPIOC_CLK_ENABLE();

 __HAL_RCC_GPIOH_CLK_ENABLE();

 __HAL_RCC_GPIOA_CLK_ENABLE();

 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */

 HAL_GPIO_WritePin(GPIOA, LD2_Pin|GPIO_PIN_10, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */

 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4|GPIO_PIN_5, GPIO_PIN_RESET);

 /*Configure GPIO pins : LD2_Pin PA10 */

 GPIO_InitStruct.Pin = LD2_Pin|GPIO_PIN_10;

 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

 GPIO_InitStruct.Pull = GPIO_NOPULL;

 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PA6 */

 GPIO_InitStruct.Pin = GPIO_PIN_6;

 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;

 GPIO_InitStruct.Pull = GPIO_NOPULL;

 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PB4 PB5 */

 GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;

 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

 GPIO_InitStruct.Pull = GPIO_NOPULL;

 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* EXTI interrupt init*/

 HAL_NVIC_SetPriority(EXTI9_5_IRQn, 0, 0);

 HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);

 HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);

 HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);

}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**

 * @brief This function is executed in case of error occurrence.

 * @retval None

 */

void Error_Handler(void)

{

 /* USER CODE BEGIN Error_Handler_Debug */

 /* User can add his own implementation to report the HAL error return state */

 __disable_irq();

 while (1)

 {

 }

 /* USER CODE END Error_Handler_Debug */

}

#ifdef USE_FULL_ASSERT

/**

 * @brief Reports the name of the source file and the source line number

 *     where the assert_param error has occurred.

 * @param file: pointer to the source file name

 * @param line: assert_param error line source number

 * @retval None

 */

void assert_failed(uint8_t *file, uint32_t line)

{

 /* USER CODE BEGIN 6 */

 /* User can add his own implementation to report the file name and line number,

   ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

 /* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi

see other posts from you related to the same question. Note that duplicated posts should be avoided. Thanks.

Rgds

BT

4 replies

Brian TIDAL
Technical Moderator
March 10, 2023

Hi,

NFC07A1_NFCTAG_WriteData writes raw data into the tag. So, the memory of your tag is basically containing "Hello the world" at offset 0 which is not an NDEF formatted data. If you want to write NDEF formatted data, make sure to use the lib_NDEF API. See en.x-cube-nfc7\Projects\NUCLEO-L476RG\Applications\NDEF_URI: this example application shows how to write an NDEF message to the ST25DV64KC EEPROM using the NDEF lib middleware.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Brian TIDAL
Technical Moderator
March 20, 2023

Hi,

please note that the language to be used on this community is English.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Schuyler
SchuylerAuthor
Associate III
March 20, 2023

Hi,

I've seen ndef. lib file, but I did not see the function of this code in the main function of STM32CUBE IDE, and the phone could not read any messages after downloading the program. Is there any relevant example that can be written into NDEF? Hi, I read the message from ndef. lib file, but I did not see the function of this code in the main function of STM32CUBE IDE, and the phone could not read any messages after downloading the program. Is there any relevant example that can be included in the information of NDEF?

The following is the code I designed. Why can't NFC Tag APP read any NDEF information

0693W00000aJKfzQAG.png

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
March 23, 2023

Hi

see other posts from you related to the same question. Note that duplicated posts should be avoided. Thanks.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.