Skip to main content
Associate
June 10, 2025
Solved

CAD resources of NUCLEO-H755ZI-Q Revision D-01

  • June 10, 2025
  • 3 replies
  • 743 views

I'm looking for CAD resources of NUCLEO-H755ZI-Q  board Revision D-01. Currently en the web-page there are for revision C-01.

 

Thanks

Best answer by Mike_ST

Hello,

Update, design files for rev D01 should be there:

CAD resources 

3 replies

Rodo
Senior
June 11, 2025

It could be that there are no changes to the PCB. You could compare the two BOMs and see what the difference is/are. That would take some time though. It would be nice to have a list of Engineering Change Notices (ECNs) on the schematic or elsewhere.

Mike_ST
Technical Moderator
June 11, 2025

Hello,

>> It could be that there are no changes to the PCB

If the revision has moved from C to D, that means PCB has been changed. It could be minor (like silkscreen) or not.

I have entered an internal ticket #211945, to see if it can be added.

 

Andrew Neil
Super User
June 11, 2025

I see both Revision D-01 and C-01:

AndrewNeil_0-1749630920735.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Mike_ST
Technical Moderator
June 11, 2025

>> I see both Revision D-01 and C-01:

Maybe I'm wrong, but I understood the request was for "MB1363 Board design project files" and "MB1363 Manufacturing files" which are only for Rev. C, because, as you mentionned, schematics for rev C and D are there.

 

Andrew Neil
Super User
June 11, 2025

Maybe:  @Lupillo_1788 just said, "CAD resources" - didn't say what "resources", specifically.

But the BoM, Manufacturing, and Design files are all dated after the D01 schematics ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.