Skip to main content
MROWL
Associate II
November 30, 2024
Solved

CAN TWO NODE DEV w/ STM32 F446/H745 using Spark Max Microcontrollers and Neo Brushless Motors

  • November 30, 2024
  • 2 replies
  • 717 views

Completed the STM CAN 2 Node tutorial and created the set up successfully. Have Spark Max and NEO motors in robot with RoboRio . However would like to do a breadboard set up less another Rio ( expensive ) . Just to function a 2 Node CAN ( micro & motors ) - Are my STM 32F446 or H745 controllers compatible . Can I dev a set up with either as a master.

Has this been done ?  Any resources or guidelines available for hardware and software? 

    2 replies

    Pavel A.
    Pavel A.Best answer
    Super User
    December 1, 2024
    MROWL
    MROWLAuthor
    Associate II
    December 1, 2024

    thanks