Skip to main content
Associate II
September 2, 2024
Question

Connecting a NUCLEO-L552ZEQ to a New haven display that uses a SSD1353

  • September 2, 2024
  • 0 replies
  • 517 views

I am mostly wondering if anyone here has ever had to code to communicate with a SSD1353 via stm32. I have used NHD documentation to connect the board in a 6800 Parallel interface. I know it is wired correctly as I connected it to my Arduino and used the company's example code that is only available for Arduino and it worked. I took that code and rewrote all of it to work on stm32 and it isn't working. Has anyone here ever written a script that I could try and use that successfully work on the SSD1353.