Associate II
July 14, 2025
Question
Custom Board Review Based on MB997E .
- July 14, 2025
- 3 replies
- 432 views
Hi ST Community,
I have developed a custom board based on the MB997E evaluation board as a reference design.
1. Could you please help me review my custom board design and schematic to identify any possible mistakes.
2. In my custom design, I have also added an external 32.768 kHz crystal oscillator for the RTC function.
Is the connection correct?
Are the load capacitors and routing appropriate?
Do I need to make any changes to ensure stable operation?
I am attaching my schematic Any suggestions or corrections would be very helpful .